Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description

CW Carrier

Add Carrier

Click this button to open a Closeddrop-down menu from which you can select a carrier to add to the setup table. The carrier is inserted above the currently selected row in the table. The maximum number of carriers is 16.

Delete Carrier

Click this button to delete the currently selected carriers in the setup table. You can highlight multiple carriers for deletion by holding down the CTRL key. You can also use the SHIFT key to select a succession (group) of carriers.

Copy Carrier

Click this button to quickly add a copy of the selected carrier to the last row in the setup table.

1. General

State

Double-click or use the drop-down menu to control the operating state of the carrier.

2. Baseband

Oversampling Ratio

This is a read only parameter. This parameter is not editable.

Baseband Sampling Rate

View the baseband sample rate. You cannot edit this cell.

Total Sample Points

View the Waveform Length, displayed in points. You cannot edit this cell.

Waveform Length is directly related to the Oversampling Ratio value selected. The higher the Oversampling Ratio, the larger the waveform.

Frequency Offset

Set the frequency offset for the carrier relative to the signal generator’s frequency setting.

The range of the parameter is coupled to the Oversampling Ratio, the Baseband Sampling Rate and the max ARB Sample Clock of the connected signal generator.

Power

Range: -60 to 0 dB

Set the carrier’s power relative to the signal generator’s amplitude setting.

Graph View

The graph view displays several different representations of the generated waveform. For more information, see Graph View.